Add the Controller

  1. In the File menu, click New to start the Controller Creation Wizard.
  2. Select the type of controller in the project.

  3. Choose the motion engine option (Pipe Network Concept or PLCopen®) and select the application template.
    See the Available Application Templates list).

  4. Click Finish.
  5. In the File menu, click Save As.
  6. Define the Project Name and its location.
  7. Click OK.

Available Application Templates